This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Query on measuring 30uA using accumulator mode

Part Number: BQ35100


HI,

Please help to confirm if BQ35100 can be used for  Li-SOCl2 Primary battery 12000mAH that for its remaining capacity measurement during operation.

Continuous load on the battery is 30uA and hourly once load current goes to 600mA(average) for a duration of few seconds.

 I want to use BQ35100 to know the % of battery capacity remaining.

Is 30uA too small to measure for BQ35100 in Accumulator mode? What is the min current can BQ35100 measure in Accumulator mode? 

Thanks