Part Number: UCC28950
Hi,
To achieve ZVS I have used shim inductor. PQ2620 core AF139 material, 33SWG conductor 30 strands, inductance 50uH.
And it is noticed that the shim inductor is heating a lot it is going beyond 100 degrees in a few minutes. I have tried at 400W as well as at 800W.
initially, I thought it is due to the minimum load issue for zvs. But the thing is that heating is increasing as loading got increased. Attaching the Vds and Vgs waveforms at 800W load.
blue is Vds(10X probe) 400V, yellow is Vgs. I think the miller plateau is still present. which means ZVS is not achieved. the case is almost similar for both the active and passive legs for 800 and 400W loads.
What will be the reason for this?