Part Number: BQ4050
Other Parts Discussed in Thread: BQ40Z50, , BQ2980, BQ77915, BQ25710, EMB1499Q, EMB1428Q
Hi,
The following E2E thread lead me to BQ4050 and BQ40z50. Can I please have some help with the implementation?
https://e2e.ti.com/support/power-management/f/196/t/871568
Hibernation
We need our battery protection IC to be able to open the charge and discharge FETs on command from the MCU, or in there is a fault. The protection IC should then keep the load removed until a charger is connected. e.g. the same as BQ2980 and BQ77915
It looks like the BQ4050/BQ40z50 ManufacturerAccess() MAC Shutdown feature will do exactly this. (1) Can you please confirm?
Section 5.4.2 on page 41 - www.ti.com/.../sluuaq3.pdf
(2) The Technical Reference manual linked above is for BQ4050, but does it also apply to BQ40z50?
System Present vs Shutdown
The SHUTDN and PRES features share a pin. (3) How do we select which feature we want to use? I couldn't find it in the datasheet.
(4) Do we need the SHUTDN feature enabled (System Present disabled) in order to use the ManufacturerAccess() MAC Shutdown feature, or is that a separate thing?
Smart Charger
We are considering BQ25710 as our smart charger because of its OTG capability. (5) In order for BQ4050/BQ40z50 and BQ25710 to interact, do they just need to be on the same SMBus, or are there more steps involved?
This is mentioned on page 24 of the BQ4050/BQ40z50 datasheets.
"Reports the appropriate charging current needed for constant current charging and the appropriate charging voltage needed for constant voltage charging to a smart charger using SMBus broadcasts" https://www.ti.com/lit/ds/symlink/bq4050.pdf#page=24
(6) How do BQ4050/BQ40z50 know what voltage and current to negotiate with BQ25710 in smart charging?
Active Balancing
(7) Can the built-in passive balancing in the BQ4050 and BQ40z50 be disabled by an MCU?
I’m told that BQ4050/BQ40z50 can be connected with EMB1428Q and EMB1499Q to add active balancing but looking through the datasheets, it doesn’t look like BQ4050/BQ40z50 have the right pins to interact with EMB1428Q/EMB1499Q. (8) How would they connect?
Kind regards,