Part Number: BQ24105-Q1
Hi TI-team
My customer have some question about FDK Recommend Charging Procedure for Back-Up Batteries In-Vehicle Applications

1. There are three different charging procedures depending on the battery voltage.
Even when not using an external MCU, does the BQ24105-Q1 decide which charging procedure to use by itself ?
2.Please tell me the content of health check.
In addition, it says "If customer need", how do you set the presence or absence of a health check ?
3.Customers are aware that the timer charging method charges at a constant current for a predetermined time.
Isn't the battery voltage checked during charging ?
Even if it is fully charged, will it continue charging until the set time expires ?
4.If a temperature abnormality occurs during charging of the timer or the engine is turned off, charging is stopped halfway, and charging is restarted, will the timer be reset ?
Or is the timer counted from the last time ?
Best Regards,
Koji Hayashi