Part Number: TPS65218D0
Other Parts Discussed in Thread: TPS65910, TPS65217, TPS650250, TPS6521825, TPS6521815, BOOSTXL-TPS65218, MSP-EXP430F5529LP, IPG-UI, TPS65218
We have a custom board based heavily off of am437x-sk-evm. The board is able to boot fine, except if the second ethernet port is not plugged in. Plugging in the cable causes an immediate reboot, but only if the USB controller has not initialized. De-initializing the USB controller at any time with the second ethernet port plugged in triggers the reboot. See the original post here: https://e2e.ti.com/support/processors/f/791/t/902314
After a large amount of trial and error, we have been able to work around the issue by disabling STRICT mode on the PMIC. After several days of probing, however, we are still unable to find any events on any of the voltage rails (DCDC1-4, LDO1). Is there anything else that STRICT changes that could be the root issue?
Also, it looks the like thresholds of STRICT changed between the EVM's B1 silicon and our D0 silicon. Has the am437x-sk-evm ever been tested using a TPS65218D0?