Part Number: UCC256302
When the burst operation is exited, dV/dt cannot be confirmed and operation is being performed by the ISNS pin.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC256302
When the burst operation is exited, dV/dt cannot be confirmed and operation is being performed by the ISNS pin.
Hello,
During normal operation, I believe you are correct that the high side FET turns on when Isns is negative.
However when both FETs turn off during burst mode their is ringing in the primary and to stop the transformer from saturating the opposite gate turns on when coming out of the burst. If the Isns polarities are incorrect the UCC256302 will adjust the timing until the high side and low side gates are triggered with the proper Isns current polarities.
So when coming out of a burst packed it is possible for the gate drive to turn-on when the Isns pin has the long polarity. However, as you waveform shows this is generally correct in three switching cycles.
Regards,
Hello,
In the waveform of the normal product sent, the gate is on when the ISNS pin voltage is high.
When you exit Burst Mode, the gate may turn on when ISNS has a long polarity. Is this the reason why the gate turns on when the ISNS pin is high?
What are the conditions under which this mode occurs?
Regards,
Hello,
I have researched this further. The ISNS pin is used to detect over current and not does not control were the HO and LO FETs turn on during normal operation. This pin monitors the current will shut down the FETs on over current conditions.
The voltage on the VCR pin actually controls the turn off of the high side and low side FETS based on a 3V common mode voltage and the voltage on RFB. Please refer to the attached slide that explains this.VCR Controls Turnoff of the FETs.pptx
The UCC256302 will monitor the switch node and turn on the HO and LO FET when zero Volt switching is detected at the switch node. Please note that delay of the Turnon of these FETs is also adjust internally by the UCC256302 to ensure there is not too much body diode conduction.
Please study your waveforms again in regards and look at the VCR pin and FB pin voltage and FB current, you should be able to determine the gate drive turnoff of the HO and LO FETs
Regards,