This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: STAT_VDPM is writable

Part Number: BQ25710

Hi,

What situation is considered when STAT_VDPM (SMBus 21h.bit7) is written by host? Other status register bit6-0 are Read only.

Regards,
Kazuto
  • Hi Kazuto-san,

    A read only status bit is latched for the event until a host read the bit. The bit will be cleared if the corresponding event is already gone when the read happens. The STAT_VDPM status bit is latched if VIN DPM happens until a write to clear the bit. The bit won't be cleared by a read. The purpose for a write to clear the bit is to let host identify whether the VIN DPM is due to the possible adaptor removal.