Part Number: BQ25606
Hi
My customer design with BQ25606, when the cell voltage discharge to 2.8V, then supply 6.5V 2A, the battery charge normal.
If change the supply voltage to 5V, the battery can not charge.
Do you have any suggestion.
Thanks
Star
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ25606
Hi
My customer design with BQ25606, when the cell voltage discharge to 2.8V, then supply 6.5V 2A, the battery charge normal.
If change the supply voltage to 5V, the battery can not charge.
Do you have any suggestion.
Thanks
Star
Star,
Please visit https://e2e.ti.com/support/power-management/f/196/t/890626 for BQ25606: Schematic Review and PCB Layout Design Tips.
Additional Information including FAQs is available http://www.ti.com/lit/an/slva924/slva924.pdf Designing A Standalone Single Cell 3-A Charger with the bq25606.
Please check if STAT pin indicate any faults and debug from there. STAT pin blinks when Charge suspend (input overvoltage, TS fault, timer fault or system overvoltage). Please also check if the input source is over-loaded, either the current exceeds the input current limit or the VBUS pin voltage falls below the input voltage limit.
Please also check if the input source is over-loaded, either the current exceeds the input current limit or the VBUS pin voltage falls below the input voltage limit.
The device then reduces the charge current until the input current falls below the input current limit and the input voltage rises above the input voltage limit. Please refer to Extract maximum power from the supply when charging a battery (http://www.ti.com/lit/an/slyt569/slyt569.pdf) for the details.
Thanks,
Ning.