Hi,
I have designed 13s Bms using three bq791500 devices. Finally I tested the Mosfet gate voltages which is around 9.5V but when the pack is loaded ( either connected to charger or discharged), Bms is turned off automatically.
1. I used 2.5milli ohm current sense resistor , all charging and discharging are under limits of 6 amps..I previously designed 10s BMS ( i used same 2.5 milli ohms without any filters), which is working well. Could you please guide me what would be the possible problem ,
》 I used 6 IRF540 Mosfets ( 3 dsg mosfets 3 chg Mosfets ), Is this the one that is creating issue? but i could see the gate voltages of 9.5V on all 6 MOSFETS. Should I change any gate resistors? Please have a look at my schematic and PCB design