Part Number: BQ24075
Hi,
EN1 -0V ,EN2 -5V,TS - 0.6V,-ILIM 1K i had only 1K instead of 1.1K in my stock, R-ISET 866 ohms.
I wanted to charge my battery at 1A because i am using 2500mah,3.7V and i want to charge my battery in 2.5 hrs only.
Input is supplied from DC power supply Input voltage :5V
My problem is current consumed from DC power supply is never exceeding 0.2A,With this current battery took almost 6 hrs. to charge from 3V to 3.8V(which is not even full capacity of battery).How to set the fast charge current to 1A, So that my battery will charge in 2.5hrs considering no Efficiency loss.
I have changed R_ISET to 590 ohms and current consumption increased to 0.3 - 0.4A sometimes going to 0.55A,But having ISET resistor 590 Ohm, battery has to charge at 1.5A, But it is not.
If the input voltage supplied is 5.9V current consumption increased from 0.2 to 1A. but the PCB is getting heated up.
Am I doing anything wrong?
Please Help.
I was not happy with response in previous thread and i am opening a new one and hoping for a solution. Link to my previous thread please go through it once : e2e.ti.com/.../3570572
Thanks & regards,
P.Akhil