Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76920, BQ78350
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQ76920, BQ78350
Hi,
Did you update the AFE Cell Map register in Data Memory when you added one more cell? Did you follow the steps in the 'Gauge Quick Start' section of the EVM User Guide? The AFE Cell Map is one of these steps.
I think this is important to resolve first because the other errors could be related.
Best regards,
Matt
I updated the data on the cells, but they are not stored in memory. in register mode, the voltage on the cells is not displayed. Chemistry and other settings are also not recorded in the registers. I figured out the calibration, it works. in the program bq769X0 Evaluation Software measurements take place and bq 920 works. I can't understand why the voltage on the cells is not displayed.
Check the voltage on the REGOUT pin. It should be 2.5V. If it is 0V, the BQ78350 is not being powered from the BQ76920 (it is in Shutdown mode) - you will need to wake the device by pressing the Boot button on the EVM.
The voltage at this terminal is 2.5 V. The current is measured at both discharge and charge. There is no measurement of voltage on the cells. I updated the cell data, but it is not stored in memory. when re-read there instead of 013 remains the value 000. it is impossible to record also the change of chemistry and data in the registers of protection. I have a suspicion that this is a bq78350 malfunction.
If you are not able to write or read from the data flash successfully, it seems there must be something wrong with the BQ78350 device. I suggest replacing the device on the EVM.
Regards,
Matt
Hi. The issue was resolved by flashing BQ350-R1 to version -R2. After that, everything worked.