Other Parts Discussed in Thread: LM5069, LM25069, LM25066, LM5066
Hello all,
Is there a TI solution for a hot swap controller with the following specs (preferably with an integrated FET)?:
Hot swapping these two input voltages:
5V in @ 30A Max
24V in @ 3A Max
The closest I've found is the LM5069 which doesn't have an integrated FET and it has min voltage of 9V, so doesn't quite meet the specifications.
Please let me know if you can find some other solution.
Thank you!
Salome