Other Parts Discussed in Thread: BQ40Z50, BQSTUDIO
Hello,
We are currently designing a battery pack featuring a bq40z50 configured for 3S. I was doing the learning cycle as following:
1/ Configure the dataflash with appropriate parameters suitable for customer's application; configure pack's chemistry and perform calibration
2/ Activate impedance track then ensure RDIS flag is set and discharge the pack in full (without triggering any protection)
3/ Relax for 5 hours and ensure both RDIS and VOK are cleared at the end of relaxation
4/ Fully charge the pack; ensure VOK is set at the beginning of charge and FC flag is set at the end of charge
5/ Relax for approximately 2 hours; ensure both VOK and RDIS are cleared at the end of relaxation
6/ Perform full discharge of the pack; ensure VOK is set at the beginning of discharge
The problem I am facing is the RDIS flag suddenly sets itself shortly after the beginning of the last discharge, thus disabling the update of the Ra tables.
Can anyone provide some insight on this matter? What are the conditions for RDIS to be set and how can I prevent it to happen again in the future? If I perform a new cycle charge/discharge with the same sample by following the above procedure, will it somehow affect the outcome of the learning?
Thank you in advance,