THe closer I look at this legacy chip, the more impressed I am. I can guess the wanswer to my question, but regardless of the reply, it looks like the bq2060 was a pioneering device in the area of flea-power design.
I see a REG output, which drives an N-Channel Depletion FET. That FET, in turn, powers even more circuitry, through an NPN Emitter-Follower. I can see that.
Here's my questions.
1) The internal REG circuit must get its power from *somewhere*. But Where is that source? Is it the RBI pin, with its diode and 10MEG Ohm in series? Is it one of the other Cell Inputs? My lands that internal regulator must be running off the earth's magnetic field.
2) The data sheet lists the REG voltage as 3.1V to 3.5V. Yet, I have reason to believe that this is actually the resultant Vcc voltage, appearing on the Source of the N-Channel Depletion FET In other words, that should be a listing for the resulatnt Vcc, especially since there is so much data about the JFET provided as a condition for assessing REG.
Please tell me the facts about these 2 issues.
Background:
I am studying a dreadful phenomena. I have a board exhibiting substantial swings in reported Load Current, even though no current is being pulled from the pack at all. This current (in the -10 to -15mA range, is highly dependent on both temperature and Pack voltage. The reported current is there, unchanged, even with Rsense shorted out.. I am therefore assessing everything connected to the regulators, etc., to account for everything I can in this system. I want to understand the function of the REG pin better, as so very much is derived from it.
I don't suppose this should matter, but I am seeing the bq2060_E207 in this board.
Yes, I have done VFC offset self-calibration three times, two of them under tightly controlled conditions.
Thanks,
Michael A. Banak