This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: Bidirectional switch for capacitive load - schematic review

Part Number: LM5069


Hi,

I'm curently trying to design a bidirectionnal switch and I decided to go for a dual back-to-back LM5069 solution. I prototyped it with 2x LM5069EVAL boards but without the dv/dt control, it worked well. 
The use case is to be able to control (switch ON / OFF) a power bus in which curent can flow in both directions.

Here are the main specs:

Voltage:
- 25V min
- 55V typical
- 60V max

Current:
-15A max

Capacitive load:
-1000uF max

The devices will be driven by a MCU by the UVLO pin.

I followed the step indicated in the excel file to design this schematic but would like a review of it.

In copy you will find the excel file completed with my specifications and the schematic I've done.


Thank you.

Best regards,

Victor G.

back_to_back_lm5069.pdfLM5069_back_to_back.xlsx