This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22919: About R_L resistance

Part Number: TPS22919
Other Parts Discussed in Thread: TPS22918,

Hello.

I asked about TPS22918, and I received the answer that R_L in the schematic of the data sheet is not the actual chip resistor to be mounted.
Is the "Load Current / Resistance (RL)" in the circuit diagram in the TPS22919 data sheet the resistance that is also not actually mounted?
Isn't it necessary to mount a chip resistor (1kΩ, etc.) between VOUT and GND?

Thank you.

  • Hashino-san,

    Just as with TPS22918, the R_L over here is to symbolize a load resistance. We use an R_L of 100Ohms, 10 Ohms, etc to characterize the device. Parameters such as timing are only possible to device once a load or test condition is setup. You can find the test conditions in the electrical characteristic for the datasheet.

    As far as your question is concerned, there is no need for a specific load resistance R_L to be placed on VOUT to GND for the device to work. This is symbolic to note a load. 

  • Thank you very much, again!

    I resolved my problem with your answer.