Dear All,
So what i am seeing is that there is an ~delay of 300uS when i read the cell data from BQ device which i don't see when using BQ EVM with BQ GUI. Can someone help me figure out why this delay is there ?
Read Cell data is divided ito differents case states to read the data and it does it as follows.
Step 1 - broadcast sample and store command
Step 2 - Read cell data 1 to 8
Step 3 - Read cell data 9 to 16
Step 4 - Read Aux data 1 to 8
Step 5 - Go back to step 2 and read data for next device in the stack.
I have cross check it several times but i can't figure out where is the delay coming from. I have also set the TX_HOLDOFF time to 0.
Your help will be very much appreciated, so can you please help ?
Kind Regards
Vikram Jain