Other Parts Discussed in Thread: BQ25505
Hello,
I am trying to figure out if the BQ25505 eval board is suitable to be used with solar panels and LiPo batteries.
I might have misunderstood the way the IC works, but isn't the 2V undervoltage protection a bit low for LiPO (my battery has something like 2.8V minimal voltage)?
Do I just connect my load on V_STOR and the LiPo on BAT_SEC or follow the example from the section 3.2.4 and connect the load in parallel with the battery ?
Best regards,
Vlad