Other Parts Discussed in Thread: BQEVSW, BQ20Z70, EV2400, BQ28400
I am running Windows 7 64-bit and am having difficulty establishing communication with the EV2400. I have version 0.9.59 bqEVSW installed for the bq20z70 and the bq20z75 fuel gauge ICs.
Upon initial connection of the EV2400, Windows did detect the EV2400, searched for, and installed a USB driver.
When I start the bqEVSW, I receive the following popup message:
The EV2300 connection could not be Initiated! Please close this program and try again.
I then click on "OK" and the bqEVSW Supported Targets window pops up. When I select my target and click on "Confirm Selection" I get the following popup window:
No USB board was detected! Please close this application first!
Then make sure that the EV2300 is connected and then restart the program!
The USB, COMM, and VOLTEN LEDs are illuminated on the EV2400