Part Number: BQ40Z50-R1
Hello,
I have successfully finished the learning cycle by SLUA777.
Max Error is 1 and Update Status is 06.
I've found a presentation from TI: Battery Management Solutions - The Final Steps to Production by Thomas Cosby; October 23, 2014
where following steps are described for the Golden File:
1. Run the Optimization Cycle to update Qmax and the Ra-table
2. Go to the Data Flash window and press the Read All button
3. Export the gg.csv file
4. Edit the gg.csv file using a text editor. e.g. Notepad. Do not use Excel.
5. Set the Update Status to 02 and set the Cycle Count to 0.
6. Load the default .srec file into the device.
7. Load the ChemID into the device.
8. Load your modified gg.csv file into the device and press the Write All button
9. Save the golden .srec file.
My question is regarding step 5:
Why is it needed to change Update Status from 06 to 02. This means Impedance Track gauging and lifetime updating is disabled (see attached screenshot)?
How to set Update Status for the Goldenfile if Impedance Track is required?