Part Number: PMP40025
Other Parts Discussed in Thread: UCC28730
Hi,
I am working on PMP40025(AC to DC flyback converter) schematics attached , I am trying to fabricate an test the reference design given in TI Website.
MOSFET in AC DC converter is controlled by UCC28730 - PSR Flyback controller.
The Vdd supply pin in UCC28730 can charge internally from rectified high voltage dc input, when it reaches 21 V, the IC is enabled.
When 21 V reached, the IC is enabled and a single pulse is observed at start up.
the controller produces continuous gate signal based( similar) on pulsed Vs input.
I gave a frequency signal( 3V, 500Hz) from a micro controller to the Vs input. but only single pulse observed, no continuous gate signal observed.
How and when it produces continuous gate signal