This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2843: Failure to turn on and drive

Part Number: UC2843

HI,

I am having a couple of problems with the UC2843. I am trying to step 12V down to 8V with output current of about 4A. 

1. It is trying to turn on but failing to do so. At the RT/CT pin I have the RT as 8.25K and CT as 1nF. 

At VFB and Comp I have a 510K resistor and a 100pF cap and for the resistor divider at VFB I have a 22k resistor as R2 (going to VCC) and 4.7K resistor as R1 (going to ground)

2. It is not providing enough current. I have a 1 ohm resistor as my sense resistor and I am using an NMOS to drive. 

Thanks