Hello. I have a design to take 60-80 volts in, and regulate it to 15V. My actual output is something around 16.4V, but that suits my application well enough as this feeds other power lines.
My issue is with my switching noise. I'm currently sitting at roughly 1.2V worth of switching noise.
I created my design based off of the LM5116 design calculator from the National site.5826.LM5116 calculator.xls
According to the calculator, I have a max average current specced for 500mA. At the moment, my load is drawing 70mA. This is a big difference in the required inductance according to the calculator. My plan was to throw a 30 Ohm, 5W resistor in series with my real load to draw the appropriate current for the inductor level, but this didn't work the way I had hoped.
Any ideas to help me with my switching noise? I've included the gates for my high side and low side FETs as well.
quick check of the schematic: R24, R25 are 0 Ohm, and R15, R16 are open.