Other Parts Discussed in Thread: LM3488
Hello All,
I am using a LM3488 to build a SEPIC converter with 5V @ 5A output. I have implemented the schematic from the WEBENCH Design Report, but I am having some problems. The converter works fine with 5V input and for very low load current. By low current I mean to power a LED and two other regulators (3.3V and 1.8V) without load.
I have a second board with a processor and other things. When I plug the processor board to the power board the output of the regulator drops to 2.5V. If I increase the input to 7.5V or above, the regulator works again. The processor board consumes approximately 100mA, that is not even close to the current that the regulator should supply.
Any ideas of what is happening?
Attached are the two schematic sheets I used in this design (one from the WEBENCH and the one I implemented).
Some of the parts I used are different from the ones referred in the WEBENCH report. Those are listed bellow.
D1 - SS5P5
Cout - EMVL160ADA471MJA0G
M1 - SI4850EY
Lin - MSS1048-682NLC
Lout - MSS1210-153MEB
Thanks,
Pedro