Other Parts Discussed in Thread: TPS54427, TPS54540, TPS5450
Hello everyone!
I would like to ask for some help regarding the usage of the TPS54427 Buck converter:
I would like to use this device to get a stable 5V output (@ max 4A) from a 6.5V power rail.
My question: Is it possible with this device? Here is why I confused a little bit:
On the product page of the device (http://www.ti.com/product/tps54427&lpos=Middle_Container&lid=Alternative_Devices) the parametrics table shows that the maximum duty cycle is 95%. However WEBENC designer says that this device is not suitable for me because the calculated DC is 83%, but the maximum DC of the device is only 65.1%.
Which is the correct maximum value? Thank you for the help in advance!