Other Parts Discussed in Thread: TPS65130
Hi,
I am evaluating TPS65130 as a power supply in one of my projects, the VPOS is always zero but VNEG is as calculated.
The schematic is exactly same as in Fig.8 of the datasheet. The following contains the details of the parts used,
Q1 -> IRF9540
D1,D2 -> ss36-e3/57t Schottky diode
L1, L2 -> 4.7uH (www.abracon.com/.../ASPI-0403.pdf)
C6,C5 -> 10nF
R1,R3 -> 1M ohm
R2,R4 -> 100K ohm
C9 was earlier open, later i added 22pF capacitor. But no output from VPOS.
C4 was totally 22uF earlier, later I removed it. C4 is open.
C10 is open.
All other values are same as in FIG.8
Observations:
After Powering ON, The P-channel Mosfet starts heating UP. BSW pin always LOW.
BSW pin always LOW.
Where have I gone wrong?