Part Number: TPS562200
Tool/software: WEBENCH® Design Tools
Hello,
i was wondering if i do need a 10kOhms resitor on the enable pin on the TPS562200 device? Using the webench tool does not giving a hint on this.
I was looking for a 3.3V output voltage @ 10V-14V input and 0.8A. I do measure around 4.7V now when using the recommended capacitors and reference voltage resistors. Thats when i started searching the fault and found the 10kOhms in the datasheet on a second image! Is this the mistake, or something different?
There are different representations: