Part Number: TPS54327
Other Parts Discussed in Thread: TPS54325
Hi, team.
My customers are considering using TPS54327.
The power supply specification is below.
① 12 V ⇒ 5.0 V / 0.6 A @ MAX
② 12 V ⇒ 3.3 V / 1.0 A @ MAX
We look at the table below and ask questions.
<Question>
1:Can I use 4.7 μH (Accuracy: ± 30%) for the inductor of ①?
※Please check both inductance value and accuracy.
2:Can I use 2.2 uH (Accuracy: ± 20%) for the inductor of ②?
※Please check both inductance value and accuracy.
3:When the answer to the above question is "No", how much accuracy is recommended for each?
Could you help us?
Best regards,
Pokkun (Masumi Sekiguchi)