Other Parts Discussed in Thread: TPS24720, TPS24750
Using TPS24720 hot-swap controller in a 12V 10A application with dV/dt control on the MOSFET Gate per the suggested alternative design example in the datasheet. Predictably, the inrush TIMER times out and shuts the MOSFET off too soon into power-up when using a Ct value of 47nF based on P-lim determined T-on (Step 4 in datasheet), but we can't find a calculation for determining Ct when using dV/dt control. Power-up succeeds by doubling the Ct value, however, this may not be enough under all conditions, and making Ct too big may risk the MOSFET SOA. The TPS24720 EVM (SLUU458A) has Ct of 68nF in parallel with a destuffed 2.2uF, and has a MOSFET Gate dV/dt network, also destuffed. Presumably the 2.2uF is stuffed when the Gate network is installed, but there is no mention of how the larger Ct is calculated.
Is there any more info for using the device with dV/dt limited gate control? I'd like to see the suggested calculation approach for Ct if there is one.