Hi,
I've designed a custom board around the LM5070-50 PoE chip, but I'm having trouble from two separate PSE devices in detecting my PD, making me believe I've done something wrong with my circuit. I've followed the reference design for the diode rectified isolated circuit almost exactly (I forgot the ground coupling cap between power and signal ground, but my understanding is this is just for EMI and noise reduction). One of the PSEs I'm using gives an error message that says undervoltage (overload) fault, making me believe my circuit is drawing too much current in some location, but to the life of me I don't see any problems and DMM probes indicate there isn't any (obvious) short. I've double checked cap and diode polarities as well.
I realize this is a pretty vague question, but I'm attaching my schematic here in the hopes that some kind soul from TI can lend a hand. The ethernet connector I'm using here (not pictured) is a bel fuse 0813-1x1t-57-f 10/100 MagJack PoE. Thanks in advance, I truly appreciate it.
Followup Question:
It seems most PoE PSE devices provide power as (+) = 0V, and (-) = -48V. I'm having trouble understanding the voltage requirements of the LM5070---is it compatible with Vin = 0, Vee = -48V?