Part Number: AM623
Other Parts Discussed in Thread: SYSCONFIG
My customer is very space limited and is therefore asking what external PU/PD are really mandatory
1. JTAG: External pull ups are needed, correct? Connect to same Power source as VDDSHV_MCU, correct?
There are no ones in the Ref Design (see SPU655i:). TDI/TDO/TCLK/EM0-1 have internal PU/PD resistors. Can you please confirm if the internal pulls are strong enough?.
2. AC9. They will not use USB1. Is the 499Ohm resistor still needed? (ref. table 6-74. in datasheet)
3. W13, W14 They will not use CSI but will use boundary scan. Can we connect VDDA_Core directly to VDD_Core without filter? SK schematics show filters.
4. GPMC_ADx Boot Mode selection: In SysConfig there is a internal Pull-seleciton possible. Is this correct or is an external resistor obligatory?
Can you please confirm (ref table 6-74) that each of these balls must be connected to the corresponding power supply(1) or VSS through separate external pull resistors to ensure the inputs associated with these balls are held to a valid logic high or low level as appropriate to select the desired device boot mode?
5. Not connected pins. For some e.g. MCASP0_AXR0 it is not described how to handle them. Which option is recommended?
A) Deselect in PinMUX (SysConfig)
B) keep selected in PinMUX and connect to GND (eg. to avoid EMC issues)
C) any other
6. Not used Pins. For some e.g. MCU_SPI0 it is not described how to handle them. Which option is recommended for Pins, that are not especailly listed in 6.4 in datasheet?
A) Not connect
B) connect somehow
Best regards,
Frank