Part Number: C6000-CGT
Other Parts Discussed in Thread: AM5729
Hi,
I've found an issue in C6000 compiler and I want to ask you if it is a "feature" or a bug.
I want to subtract two 32bit signed numbers and because the result could be bigger than 32bit signed variable, I want to have the result in 40bit variable. Thus I have written the code below and found out that retyping 32bit signed variable to 40bit signed variable actually doesn't work.
My compiler is: C6000 8.3.11
My hardware is: AM5729 C66x core
The code below presents some ways how to subtract two numbers:
result = -1 - (-2,147,483,648) = 2,147,483,647
Please find the result values in the comments at the end of a line.
You can see that the code works if subtraction is between two int32_t numbers or between two int40_t numbers, but it doesn't work if the subtraction is between the first int40_t variable and the second int32_t variable. I guess it is because of non working retyping (int40_t)variable32bit
The code:
int40_t result;
int32_t a32 = 0xFFFFFFFF;
int32_t b32 = 0x80000000;
int40_t a40 = 0xFFFFFFFFFFi40;
int40_t b40 = 0xFF80000000i40;
result = a32 - b32; // 0x007FFFFFFF
result = (int40_t)a32 - (int40_t)b32; // 0x007FFFFFFF
result = a40 - (int40_t)b32; // 0xFF7FFFFFFF
result = (int40_t)a32;
result -= (int40_t)b32; // 0xFF7FFFFFFF
result = a40 - b40; // 0x007FFFFFFF
result = a40;
result -= b40; // 0x007FFFFFFF
So, the question is if I don't understand something or it is a bug in C6000 compiler?