This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BEAGL-HUESO-NEGRO:BEAGLEBONE BLACK, UNDEFINED PORT UART

Part Number: BEAGL-BONE-BLACK

I need help with the Beaglebone Black, i require use the port UART as serial port, but when i use the command setserial -g /dev/ttyS[012345] in the terminal Debian los tty1,2,3,4,5 have in the value port 0x0000, undefined. As conclution i need defined this ports, i attach a image.

well i have another question, the image of the SO Debian that you have on your website generates a very small (3,5 GB) virtual size for the system, do you have a way to increase the size?