Tool/software:
in China customer, they use AM5716 PRUSS network port,
sdk 6.3
the PRUSS network is configured with the real-time CORE, occasionally there are network traffic storm in the network,
and received by the PRUSS port and passed up to the real-time M4 core, cause M4 core crash,
is there any solution in the PRUSS MAC to filter these un-necessary traffic based on the MAC address or other rules?
customer has tried following confguration,

ICSS_EMAC_firmware_feature_ctrl

please help check if this can work to filter traffic
Thanks
Semon