Part Number: AM625
Tool/software:
SOC_UID is a device specific identifier calculated by ROM based on "KEK of the device which is unique to every single device, plus other ROM mata-data structure".
- unique per SoC and persistent
- available on HS-FS and HS-SE
- multiple usages: unique binding to enable JTAG unlock on HS-SE; unique serial number for SoC.
There're several ways to retrieve SOC_UID as listed
https://software-dl.ti.com/tisci/esd/latest/6_topic_user_guides/secure_debug.html#retrieveing-soc-uid
1/. ROM
- Reported by ROM from ROM functional boot flow, i.e. peripheral boot modes like UART, USB-DFU
- JTAG in ROM WIR boot flow
2/. TIFS
- TISCI API