Part Number: AM6421
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
The AM64x processor family is able to support a total of 4 PRU_ICSSG Ethernet ports and 2 CPSW Ethernet ports. However, due to pinmux restrictions, only a maximum of 5 Ethernet ports can be configured at a given time. This, in theory, can be any combination of PRU_ICSSG or CPSW Ethernet ports. However, there are potentially additional pinmux restrictions depending on the MAC interface mode that is being used since the number of pins required for each interface mode is different.
For AM64x, the PRU_ICSSG Ethernet ports can be configured in RGMII or MII interface mode and the CPSW Ethernet ports can be configured in RGMII or RMII interface mode. What combination of these interface modes are valid (i.e. do not introduce a pinmux error)?