Part Number: AM62L
Tool/software:
HI TI experts,
Can you provide more inputs on the RTC Clock Signal as below
1. Use cases
2. Connection when not used
3. Using crystal or Oscillator
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62L
Tool/software:
HI TI experts,
Can you provide more inputs on the RTC Clock Signal as below
1. Use cases
2. Connection when not used
3. Using crystal or Oscillator
HI Board designers,
1. Use cases
A 32.768 KHz crystal or oscillator is recommended when the processor is configured for
RTC only mode
RTC + IO + DDR self-refresh mode
2. Connection when not used
32.768 KHz crystal or oscillator is optional when low power modes are not used.
Refer LFOSC0 Not Used section of the data sheet to connect the clock input when not used
3. Using crystal or Oscillator
Refer LFOSC0 Internal Oscillator Clock Source when crystal is used
Refer LFOSC0 LVCMOS Digital Clock Source section when using oscillator
Regards,
Sreenivasa
HI Board designers,
Refer below FAQ for additional inputs.
Regards,
Sreenivasa