Part Number: AM62P
Tool/software:
Hi TI Expeets,
Can you provide information for AM62P HS400 support.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM62P
Tool/software:
Hi TI Expeets,
Can you provide information for AM62P HS400 support.
HI Board Designers,
Ther recommendation is to source VDDR_CORE from the same source as VDD_CORE when operating VDD_CORE at 0.85V. I do not see an issue with sourcing VDDR_CORE from a different source as long as they ensure there is no operating condition that allows the potential applied to VDDR_CORE to be greater than the potential applied to VDD_CORE + 0.18V during power-up or power-down. We encourage customers to use the same source for VDDR_CORE and VDD_CORE when operating VDD_CORE at 0.85V to eliminate this concern.
Planned updates to support HS400:
The VDDA_0P85_DLL_MMC0 and VDD_MMC0 power rails, connected to their own pins 1J1 and 1K3 respectively, will be connected to the same net as the
VDDR_CORE power rail being sourced from pins 1C8, 1E5, and 1H3. This change combines the VDDR_CORE, VDD_MMC0, and VDDA_0P85_DLL_MMC0 power rails inside the package, where the three power rails will share pins 1C8, 1E5, 1H3, 1J1, and 1K3. I plan to assign the name “VDDR_CORE” to all five pins, and update the signal descriptions to include all three power rails.
This change will create a problem for any customers that is not using MMC0 and they connected the VDDA_0P85_DLL_MMC0 and VDD_MMC0 power rails
to the same source as VDD_CORE, as instructed in the previous datasheet. This PCB connectivity will short the 0.75V and 0.85V power supplies together
via our new package if they were to install a new package.
The change will also create a problem for systems designed to use two 0.85V power supplies, where one 0.85V power supply is sourcing the
VDDA_0P85_DLL_MMC0 and VDD_MMC0 power rails and the other 0.85V power supply is sourcing the VDDR_CORE power rail.
This PCB connectivity will short the two 0.85V power supplies together via our new package if they were to install a new package.
Suggested changes to the schematics
The recommendation is to connect VDDA_0P85_DLL_MMC0 and VDD_MMC0 power rails to the same power source that is connected to VDDR_CORE
Layout Guidelines
The FAQ is being updated. Please review the FAQ for updates.
Note:
The updated data sheet is available on TI.com
Data sheet
Look for AM62P Datasheet
Regards,
Sreenivasa
HI Board Designers,
The updated data sheet is available on TI.com
Data sheet
Look for AM62P Datasheet




Regards,
Sreenivasa
HI Board Designers,

Note:
The picture above is for understanding the changes.
VDDA_0P85_DLL_MMC0 (1J1) and VDD_MMC0 (1K3) power rails are named as VDDR_CORE and connected to the same power source that was sourcing power to VDDR_CORE pins 1C8, 1E5, and 1H3.
Regards,
Sreenivasa
HI Board Designers,
The design guidelines are now available on TI.com
https://www.ti.com/lit/an/spradp5/spradp5.pdf
AM62Px eMMC HS400 Board Design and Simulation Guidelines
Regards,
Sreenivasa