Other Parts Discussed in Thread: OMAP-L137
Hello, in my project I was trying to boot from the flash memory and faced the problem. So, I decided to observe a booting process without a GEL file.
I am using ARM9_intvecs.asm, ARM9_initstack.asm, ARM9_handler.asm and boot.asm for booting routine. I am trying to debug my program from the very beginning (from the entry point). My entry point in linker config file is _init_stack. And I found the problem - in this code all is ok, untill the jump to c_int00. On the instruction "LDR PC, c_int00" debugger says that "No source available for "0x0". What am I doing wrong?
(I have omap-l137 evm from spectrum digital and use CSL macros.)
;*----------------------------------------------------------------------------- ;* Source Location: OMAPL1x/support/src/ ;* File: ARM9_initstack.asm ;* ;* Copyright (C) 2010 Texas Instruments Incorporated - http://www.ti.com/ ...... ...... ;* ;* initstack.asm ;* ;* If using the RTS library from the TMS470 Code Generation Tools 4.6.3 or ;* earlier, include this file (use function _init_stack as an entry point) ;* to initialize the privileged mode stacks. ;* ;* This module performs the following actions: ;* 1) Allocates the stack and initializes the stack pointer for SVC, ;* IRQ, & FIQ mode ;* 2) Calls the normal initial boot routine (_c_int00) ;* ;*----------------------------------------------------------------------------- ; Global symbols defined here .global _c_int00 .global _init_stack ;**************************************************************************** ;* DEFINE PRIVILEGED MODE STACKS: SVC, IRQ, & FIQ ;**************************************************************************** __SVC_STACK_SIZE:.set 0x1000 __IRQ_STACK_SIZE:.set 0x1000 __FIQ_STACK_SIZE:.set 0x1000 __svc_stack:.usect ".svcstack", __SVC_STACK_SIZE, 4 __irq_stack:.usect ".irqstack", __IRQ_STACK_SIZE, 4 __fiq_stack:.usect ".fiqstack", __FIQ_STACK_SIZE, 4 ;**************************************************************************** ;* FUNCTION DEF: _init_stack ;**************************************************************************** _init_stack:.asmfunc ; SET TO SVC MODE MRS R0, CPSR BIC R0, R0, #0x1F ORR R0, R0, #0x13 MSR CPSR_CF, R0 ; INITIALIZE THE SVC MODE STACK LDR SP, c_svc_stack LDR R0, c_SVC_STACK_SIZE ADD SP, SP, R0 ; SET TO IRQ MODE MRS R0, CPSR BIC R0, R0, #0x1F ORR R0, R0, #0x12 MSR CPSR_CF, R0 ; INITIALIZE THE IRQ MODE STACK LDR SP, c_irq_stack LDR R0, c_IRQ_STACK_SIZE ADD SP, SP, R0 ; SET TO FIQ MODE MRS R0, CPSR BIC R0, R0, #0x1F ORR R0, R0, #0x11 MSR CPSR_CF, R0 ; INITIALIZE THE FIQ MODE STACK LDR SP, c_fiq_stack LDR R0, c_FIQ_STACK_SIZE ADD SP, SP, R0 ; Continue to _c_int00 LDR PC, c_int00 .endasmfunc ;**************************************************************************** ;* CONSTANTS USED BY THIS MODULE ;**************************************************************************** c_int00 .long _c_int00 c_svc_stack .long __svc_stack c_irq_stack .long __irq_stack c_fiq_stack .long __fiq_stack c_SVC_STACK_SIZE .long __SVC_STACK_SIZE c_IRQ_STACK_SIZE .long __IRQ_STACK_SIZE c_FIQ_STACK_SIZE .long __FIQ_STACK_SIZE