Part Number: TDA4VM
Dear Sir/Mam,
We have a external switch BCM 89551 connected to the TDA4 internal switch over port 8 of external switch. We are not using the MDIO interface at all.
Do need to add the node for this external switch 89551 in the device tree ? If yes, than at the moment i am not able to find the corresponding binding for it.
Also , do i need to add it in U-boot dtsi too ?
Please see the attached picture for internal switch