hi the community,
I'am using an EZDSP TMS320VC5505 in an optical measurement equipment. On the equipment we use the second port of the FTDI 2232 chips to comminucate with a pc through an usb serial port.
So we develop a DSP application using Code composer studio and the debugger works fine through the jtag using the first serial line of the FT2232. We develop an application on the pc side interfacing the instrument using the second serial line of the FT2232.
We develop on a sony VAIO PC platform running windows7. We installed drivers from FTDI to get both serial lines working together. And for a while everything was working fine.
Few days ago, we had a problem with the usb serial port driver. Very difficult to make a diagnostic of the problem so we tried to reinstall the drivers but we always get a code 39 error after the installation completes? I have uninstalled the drivers : usb serial converter and usb serial port and afterward i tried reinstalling the drivers but i always get the same problem.
If somebody had a good idea maybe it could help me.
Manu