This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-AM243: AM243x

Part Number: LP-AM243

Dear TI colleagues,

       I want to ask a question about Launch Pad of AM243x(Schematic name:PROC109E1_SCH):

we can see the picture below: VDDSHV5 is the power supply of mmc/SD,but  only connect to CAP_CDDSHV_MMC1,

no external supply,Is there a power conversion circuit for the emmc module inside the chip?

If so, for MMC 1.8V and 3.3V, are there corresponding registers to configure the desired level?