Other Parts Discussed in Thread: OMAP3530
Hi,
I saw the files and I am using OMAP35X board REV D
I am using TI_SDCard_boot_utility for record MLO, EBOOTSD.NB0 and NK.BIN in SD card. And I am using EVMFlash3530 for download TIEVM3530-nand.raw in flash address 0x20000000.
When I put SW4 switch 2 and 4 ON I can communicate by UART3 with serial port Monitor, than I appear in serial port
....40.T..................................................
.Texas Instruments Windows CE NAND X-Loader for EVM 3530
.Built Apr 6 2011 at 17:17:49
.Version 6.14.01
..
.Jumping to bootloader
.Microsoft Windows CE Bootloader Common Library Version 1.4 Built Apr 6 2011 17:12:17
.
.Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Apr 6 2011 at 17:17:39
.EBOOT Version 1.1, BSP 6.14.01
.
.TI OMAP3530 Version 0x2b7ae02f (ES2.1)
TPS659XX Version 0x50 (Unknown)
.System ready!
Preparing for download...
.INFO: Predownload....
.Checking bootloader blocks are marked as reserved (Num = 14)
.INFO: Boot configuration found
.OALFlashStoreOpen: 2048 blocks, 64 sectors/block
.OALFlashStoreOpen: 2048 bytes/sector, 14 reserved blocks
.>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
.Hit space to enter configuration menu 5...
.Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
.--------------------------------------------------------------------------------
. Main Menu
--------------------------------------------------------------------------------
. [1] Show Current Settings
. [2] Select Boot Device
. [3] Select KITL (Debug) Device
[4] Network Settings
. [5] Flash Management
. [6] Set Device ID
. [7] Save Settings
. [8] Enable/Disable OAL Retail Messages
. [0] Exit and Continue
.
I send [2] and choose [3] SD Card File.
. Select Boot Device
.--------------------------------------------------------------------------------
. [1] LAN9115 MAC
[2] USBFn RNDIS
. [3] SDCard FILE
. [4] NK from NAND
. [0] Exit and Continue
.
. Selection (actual SDCard FILE ):
So if I reset the board LCD show the image below and backlight turn off.

If I change the SW4 switch for 1, 2 and 3 ON and restart the board nothing happen and backlight be ON.
If I choose boot [4] NK from NAND appear the message. (SW4 switch 2 and 4 ON)
.Load NK image from flash memory
.ERROR: Image signature not found
Please tell me what I am doing wrong
What I have to do?
Thanks