Other Parts Discussed in Thread: TVP5146
Dear All,
I have a omap3evm board and I was able to capture and display the composite input using the demo application saMmapLoobpback. I also have S-Video and Component input sources. I know the TVP5146 decoder in omap3evm can support only one type of input acquisition at a time. Whenever I run the application, the composite input gets selected always. How can I able to select the other two inputs. For example, I would first like to display the composite input for the first 5 minutes, the next 5 minutes for S-Video input and the third 5 minutes for Component input. I know it is possible but I am not aware of how to select the sources based on our needs. It would be very helpful if someone can point me to the solution.
Regards,
Krishnan.