Part Number: TMDSICE3359
Hi,
I have built the Kernel and modules with option CONFIG_HSR=y. I am trying to run the commands listed here https://software-dl.ti.com/processor-sdk-linux/esd/docs/latest/linux/Industrial_Protocols_HSR_PRP.html
I am getting the following error:
root@am335x-evm:~# ifconfig eth0 0.0.0.0 down && ifconfig eth1 0.0.0.0 down
[ 73.066232] cpsw 4a100000.ethernet eth0: Link is Down
[ 73.145642] cpsw 4a100000.ethernet eth1: Link is Down
root@am335x-evm:~# ifconfig eth0 hw ether 70:FF:76:1C:0E:8C && ifconfig eth1 hw
ether 70:FF:76:1C:0E:8C
root@am335x-evm:~# ethtool -K eth0 hsr-rx-offload on && ethtool -K eth1 hsr-rx-o
ffload on
Could not change any device features
root@am335x-evm:~#
Pls find attached the boot log
0 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... *** Warning - bad CRC, using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: eth0: ethernet@4a100000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
4665856 bytes read in 397 ms (11.2 MiB/s)
61547 bytes read in 10 ms (5.9 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df23000, end 8df3506a ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.4.106-g023faefa70 (chanderbgoel@chanderbgoel-VirtualBox.ti.com) (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 PREEMPT Thu Nov 25 15:39:53 IST 2021
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM3359 ICE-V2
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64706
[ 0.000000] Kernel command line: console=ttyO3,115200n8 root=PARTUUID=97bf3d08-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 194184K/261120K available (9216K kernel code, 295K rwdata, 3100K rodata, 1024K init, 254K bss, 17784K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] random: get_random_bytes called from start_kernel+0x2b4/0x470 with crng_init=0
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000022] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000049] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000061] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000416] timer_probe: no matching timers found
[ 0.000644] Console: colour dummy device 80x30
[ 0.000685] WARNING: Your 'console=ttyO3' has been replaced by 'ttyS3'
[ 0.000694] This ensures that you still see kernel messages. Please
[ 0.000701] update your kernel commandline.
[ 0.000759] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.058650] pid_max: default: 32768 minimum: 301
[ 0.058947] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.058966] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.060101] CPU: Testing write buffer coherency: ok
[ 0.060184] CPU0: Spectre v2: using BPIALL workaround
[ 0.061236] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.061427] rcu: Hierarchical SRCU implementation.
[ 0.061533] EFI services will not be available.
[ 0.061988] devtmpfs: initialized
[ 0.077491] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.077979] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.078019] futex hash table entries: 256 (order: -1, 3072 bytes, linear)
[ 0.082929] pinctrl core: initialized pinctrl subsystem
[ 0.083908] DMI not present or invalid.
[ 0.084484] NET: Registered protocol family 16
[ 0.087531] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.117346] l3-aon-clkctrl:0000:0: failed to disable
[ 0.120012] cpuidle: using governor ladder
[ 0.120057] cpuidle: using governor menu
[ 0.143293] No ATAGs?
[ 0.143307] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.165474] debugfs: Directory '49000000.edma' with parent 'dmaengine' already present!
[ 0.165518] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.168144] iommu: Default domain type: Translated
[ 0.171480] SCSI subsystem initialized
[ 0.172132] mc: Linux media interface: v0.10
[ 0.172186] videodev: Linux video capture interface: v2.00
[ 0.172311] pps_core: LinuxPPS API ver. 1 registered
[ 0.172322] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.172350] PTP clock support registered
[ 0.172396] EDAC MC: Ver: 3.0.0
[ 0.173887] Advanced Linux Sound Architecture Driver Initialized.
[ 0.175434] clocksource: Switched to clocksource timer1
[ 0.186612] thermal_sys: Registered thermal governor 'fair_share'
[ 0.186624] thermal_sys: Registered thermal governor 'bang_bang'
[ 0.186647] thermal_sys: Registered thermal governor 'step_wise'
[ 0.186657] thermal_sys: Registered thermal governor 'user_space'
[ 0.186665] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.187377] NET: Registered protocol family 2
[ 0.188331] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096 bytes, linear)
[ 0.188376] TCP established hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.188413] TCP bind hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.188449] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.188581] UDP hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.188608] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes, linear)
[ 0.188815] NET: Registered protocol family 1
[ 0.189553] RPC: Registered named UNIX socket transport module.
[ 0.189570] RPC: Registered udp transport module.
[ 0.189578] RPC: Registered tcp transport module.
[ 0.189585] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.189606] PCI: CLS 0 bytes, default 64
[ 0.190754] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.192411] Initialise system trusted keyrings
[ 0.192803] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.200002] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.201008] NFS: Registering the id_resolver key type
[ 0.201064] Key type id_resolver registered
[ 0.201075] Key type id_legacy registered
[ 0.201134] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.202061] Key type asymmetric registered
[ 0.202077] Asymmetric key parser 'x509' registered
[ 0.202141] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.202155] io scheduler mq-deadline registered
[ 0.202165] io scheduler kyber registered
[ 0.209127] OMAP GPIO hardware version 0.1
[ 0.239965] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.259142] GPIO line 100 (PR1_MII_CTRL) hogged as output/high
[ 0.259182] GPIO line 106 (MUX_MII_CTL1) hogged as output/high
[ 0.269584] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 0.340919] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.347057] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 44, base_baud = 3000000) is a 8250
[ 0.973035] printk: console [ttyS3] enabled
[ 0.980684] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 0.987099] random: fast init done
[ 0.990770] random: crng init done
[ 1.017498] brd: module loaded
[ 1.029895] loop: module loaded
[ 1.040241] spi-nor spi0.0: found s25fl064k, expected w25q64
[ 1.046156] spi-nor spi0.0: s25fl064k (8192 Kbytes)
[ 1.051113] 4 fixed-partitions partitions found on MTD device spi0.0
[ 1.057530] Creating 4 MTD partitions on "spi0.0":
[ 1.062356] 0x000000000000-0x000000080000 : "u-boot-spl"
[ 1.076433] 0x000000080000-0x000000180000 : "u-boot"
[ 1.086387] 0x000000180000-0x0000001a0000 : "u-boot-env"
[ 1.096366] 0x0000001a0000-0x000000800000 : "misc"
[ 1.108165] libphy: Fixed MDIO Bus: probed
[ 1.175537] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.183249] libphy: 4a101000.mdio: probed
[ 1.190355] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver TI TLK10X 10/100 Mbps PHY
[ 1.200074] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver TI TLK10X 10/100 Mbps PHY
[ 1.209990] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.216490] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.221856] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.229193] cpsw 4a100000.ethernet: Detected MACID = 00:35:ff:78:be:90
[ 1.236875] cpsw 4a100000.ethernet: cpsw: Detected MACID = 00:35:ff:78:be:92
[ 1.246294] i2c /dev entries driver
[ 1.254308] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.262127] sdhci: Secure Digital Host Controller Interface driver
[ 1.268402] sdhci: Copyright(c) Pierre Ossman
[ 1.286329] omap_hsmmc 47810000.mmc: RX DMA channel request failed
[ 1.292874] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.301191] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.312551] NET: Registered protocol family 10
[ 1.318612] Segment Routing with IPv6
[ 1.322383] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.329194] NET: Registered protocol family 17
[ 1.334028] Key type dns_resolver registered
[ 1.338740] omap_voltage_late_init: Voltage driver support not added
[ 1.345836] Loading compiled-in X.509 certificates
[ 1.385666] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.396794] vrtc: supplied by vbat
[ 1.402412] vio: supplied by vbat
[ 1.408364] vdd_mpu: supplied by vbat
[ 1.414555] vdd_core: supplied by vbat
[ 1.421367] vdig1: supplied by vbat
[ 1.426248] vdig2: supplied by vbat
[ 1.431086] vpll: supplied by vbat
[ 1.435901] vdac: supplied by vbat
[ 1.440670] vaux1: supplied by vbat
[ 1.445550] vaux2: supplied by vbat
[ 1.450391] vaux33: supplied by vbat
[ 1.455324] vmmc: supplied by vbat
[ 1.460086] vbb: supplied by vbat
[ 1.464694] pca953x 0-0041: 0-0041 supply vcc not found, using dummy regulator
[ 1.472141] pca953x 0-0041: using no AI
[ 1.503057] Console: switching to mono frame buffer device 12x2
[ 1.536484] ssd1307fb 0-003c: fb0: Solomon SSD1307 framebuffer device registered, using 192 bytes of video memory
[ 1.547091] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.588595] hctosys: unable to open rtc device (rtc0)
[ 1.595129] ALSA device list:
[ 1.598584] No soundcards found.
[ 1.603232] Waiting for root device PARTUUID=97bf3d08-02...
[ 1.666980] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.680911] mmc0: new high speed SDHC card at address aaaa
[ 1.688109] mmcblk0: mmc0:aaaa SC16G 14.8 GiB
[ 1.696681] mmcblk0: p1 p2
[ 2.143455] EXT4-fs (mmcblk0p2): recovery complete
[ 2.149713] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.158000] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.174887] devtmpfs: mounted
[ 2.179992] Freeing unused kernel memory: 1024K
[ 2.185185] Run /sbin/init as init process
[ 2.524213] systemd[1]: System time before build time, advancing clock.
[ 2.580421] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[ 2.603178] systemd[1]: Detected architecture arm.
Welcome to Arago 2020.09!
[ 2.660406] systemd[1]: Set hostname to <am335x-evm>.
[ 3.642352] systemd[1]: system-getty.slice: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 3.655227] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 3.668964] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 3.708460] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.750215] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.787791] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 3.826294] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 3.867059] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 3.896270] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.935917] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 3.966418] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 4.002818] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 4.046271] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 4.106567] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 4.147262] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.249538] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[ 4.259537] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.297127] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.334032] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.377166] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.418187] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.456838] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[ 4.478649] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.523231] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.601643] systemd[1]: Mounting Temporary Directory (/tmp)...
Mounting Temporary Directory (/tmp)...
[ 4.654140] systemd[1]: Starting Create list of static device nodes for the current kernel...
Starting Create list of st…odes for the current kernel...
[ 4.718975] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 4.775020] systemd[1]: Started Hardware RNG Entropy Gatherer Daemon.
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 4.835196] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 4.886237] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 4.933389] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.006972] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 5.066993] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.110002] cryptodev: loading out-of-tree module taints kernel.
[ 5.155915] systemd[1]: Starting udev Coldplug all Devices...
[ 5.162984] cryptodev: driver 1.10 loaded.
Starting udev Coldplug all Devices...
[ 5.224076] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 5.328259] systemd[1]: Started Start psplash boot splash screen.
[ OK ] Started Start psplash boot splash screen.
[ 5.366802] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 5.387005] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 5.417073] systemd[1]: Mounted Kernel Debug File System.
[ OK ] Mounted Kernel Debug File System.
[ 5.457345] systemd[1]: Mounted Temporary Directory (/tmp).
[ OK ] Mounted Temporary Directory (/tmp).
[ 5.499578] systemd[1]: Started Create list of static device nodes for the current kernel.
[ OK ] Started Create list of sta… nodes for the current kernel.
[ 5.575768] systemd[1]: Started Load Kernel Modules.
[ OK ] Started Load Kernel Modules.
[ 5.620035] systemd[1]: Started Remount Root and Kernel File Systems.
[ OK ] Started Remount Root and Kernel File Systems.
[ 5.668227] systemd[1]: Condition check resulted in FUSE Control File System being skipped.
[ 5.735963] systemd[1]: Mounting Kernel Configuration File System...
Mounting Kernel Configuration File System...
[ 5.800769] systemd[1]: Started Start psplash-systemd progress communication helper.
[ OK ] Started Start psplash-syst…progress communication helper.
[ 5.852237] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[ 5.892517] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 5.946854] systemd[1]: Condition check resulted in Create System Users being skipped.
[ 5.990872] systemd[1]: Starting Create Static Device Nodes in /dev...
Starting Create Static Device Nodes in /dev...
[ 6.051050] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting Flush Journal to Persistent Storage...
Starting udev Kernel Device Manager...
[ 6.628036] systemd-journald[78]: Received client request to flush runtime journal.
[ OK ] Mounted /media/ram.
[ OK ] Mounted /var/volatile.
[ OK ] Started Flush Journal to Persistent Storage.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Reached target System Time Synchronized.
[ 9.511029] input: gpio-decoder as /devices/platform/gpio-decoder/input/input0
[ 9.941453] remoteproc remoteproc0: wkup_m3 is available
[ OK ] Started udev Coldplug all Devices.
[ OK ] Reached target System Initialization.
[ 10.618124] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ OK ] Started Daily rotation of log files omap_rtc 44e3e000.rtc: registered as rtc0
[0m.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on dropbear.socket.
[ OK ] Reached target Sockets.
[ 11.017834] remoteproc remoteproc0: powering up wkup_m3
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
[ 11.226024] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 243196
[ 11.234444] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 11.234469] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
Starting Reboot and dump vmcore via kexec...
Starting rc.pvr.service...
Starting Login Service...
[ OK ] Started IPv6 Packet Filtering Framework.
[ OK ] Started IPv4 Packet Filtering Framework.
[ OK ] Started Reboot and dump vmcore via kexec.
[ 13.493162] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 0
[ 13.826944] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
[ OK ] Started rc.pvr.service.
[ 15.713183] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 15.814692] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 15.946431] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 16.008439] PM: bootloader does not support rtc-only!
[ 24.823877] remoteproc remoteproc1: 4a334000.pru is available
[ 24.933919] pru-rproc 4a334000.pru: PRU rproc node /ocp/interconnect@4a000000/segment@0/target-module@300000/pruss@0/pru@34000 probed successfully
[ 25.113666] remoteproc remoteproc2: 4a338000.pru is available
[ 25.133770] pru-rproc 4a338000.pru: PRU rproc node /ocp/interconnect@4a000000/segment@0/target-module@300000/pruss@0/pru@38000 probed successfully
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gstreamer1.0-libav
gzip
hidapi
less
libasm1
libbfd
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp10
libidn2-0
libmpc3
libmpfr6
libreadline-dev
libreadline8
libunistring2
m4-dev
m4
make
nettle
pdm-anomaly-detection
tar
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ OK ] Started Login Service.
[ OK ] Created slice system-systemd\x2dbacklight.slice.
[ OK ] Created slice system-systemd\x2dfsck.slice.
[ OK ] Created slice system-weston.slice.
[ OK ] Reached target Network (Pre).
[ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
Starting Load/Save Screen …ess of backlight:ssd1307fb0...
Starting File System Check on /dev/mmcblk0p1...
Starting Network Service...
Starting weston.service...
[ OK ] Started Load/Save Screen B…tness of backlight:ssd1307fb0.
[ OK ] Started weston.service.
Starting Matrix GUI...
Starting telnetd.service...
[ OK ] Started File System Check on /dev/mmcblk0p1.
[ OK ] Started Matrix GUI.
[ OK ] Started telnetd.service.
[ OK ] Started Network Service.
[ 33.590603] net eth1: initializing cpsw version 1.12 (0)
[ 33.746378] TI TLK10X 10/100 Mbps PHY 4a101000.mdio:03: attached PHY driver [TI TLK10X 10/100 Mbps PHY] (mii_bus:phy_addr=4a101000.mdio:03, irq=POLL)
Mounting /run/media/mmcblk0p1...
Starting Wait for Network to be Configured...
[ 33.955705] cpsw 4a100000.ethernet: initializing cpsw version 1.12 (0)
Starting Network Name Resolution...
[ 34.145858] TI TLK10X 10/100 Mbps PHY 4a101000.mdio:01: attached PHY driver [TI TLK10X 10/100 Mbps PHY] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL)
[ OK ] Mounted /run/media/mmcblk0p1.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Network.
[ OK ] Reached target Host and Network Name Lookups.
Starting Avahi mDNS/DNS-SD Stack...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Permit User Sessions.
[ 35.926920] cpsw 4a100000.ethernet eth1: Link is Up - 100Mbps/Full - flow control off
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ 35.983174] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[ OK ] Created slice system-systemd\x2dcoredump.slice.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Reached target Login Prompts.
[ 36.334972] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control off
[ 36.371906] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Starting Synchronize System and HW clocks...
[ OK ] Started Weston Wayland Compositor.
[ OK ] Started Process Core Dump (PID 798/UID 0).
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
[ OK ] Started User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ OK ] Started Synchronize System and HW clocks.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS3
Arago 2020.09 am335x-evm ttyS3
am335x-evm login: root
Last login: Mon May 24 08:05:45 UTC 2021
root@am335x-evm:~# ifconfig eth0 0.0.0.0 down && ifconfig eth1 0.0.0.0 down
[ 73.066232] cpsw 4a100000.ethernet eth0: Link is Down
[ 73.145642] cpsw 4a100000.ethernet eth1: Link is Down
root@am335x-evm:~# ifconfig eth0 hw ether 70:FF:76:1C:0E:8C && ifconfig eth1 hw
ether 70:FF:76:1C:0E:8C
root@am335x-evm:~# ethtool -K eth0 hsr-rx-offload on && ethtool -K eth1 hsr-rx-o
ffload on
Could not change any device features
root@am335x-evm:~# root@am335x-evm:~# ifconfig eth0 0.0.0.0 down && ifconfig eth1 0.0.0.0 down
s Down
-sh: root@am335x-evm:~#: command not found
root@am335x-evm:~# ifconfig eth0 hw ether 70:FF:76:1C:0E:8C && ifconfig eth1 hw
ether 70:FF:76:1C:0E:8C
root@am335x-evm:~# [ 73.066232] cpsw 4a100000.ethernet eth0: Link is Down
-sh: [: missing `]'on && ethto
ol -K eth1 hsr-rx-o
ffload on
Could not change any device features
root@am335x-evm:~#
Please Help
Regards,
Chander