This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: add our own kernel

Part Number: TDA4VM

HI:

I have a question about dl_demos. when using our own models for seg, models have been transed successfully with the tidl exe. When adding our own kernel to create and veritify the graph, we have a problem:

11800.345377 s: VX_ZONE_ERROR:[ownContextSendCmd:789] Command ack message returned failure cmd_status: -7

11800.345432 s: VX_ZONE_ERROR:[ownContextSendCmd:823] tivxEventWait() failed.

11800.345477 s: VX_ZONE_ERROR:[ownNodeKernelInit:557] Target kernel, TIVX_CMD_NODE_CREATE failed for node MultitaskPostProcNode

11800.345546 s: VX_ZONE_ERROR:[ownNodeKernelInit:558] Please be sure the target callbacks have been registered for this core

11800.345616 s: VX_ZONE_ERROR:[ownNodeKernelInit:559] If the target callbacks have been registered, please ensure no errors are occurring within the create callback of this kernel

11800.345730 s: VX_ZONE_ERROR:[ownGraphNodeKernelInit:583] kernel init for node 1, kernel com.ti.img_proc.multitask.postprocess ... failed !!!

11800.345815 s: VX_ZONE_ERROR:[vxVerifyGraph:2046] Node kernel init failed

11800.345867 s: VX_ZONE_ERROR:[vxVerifyGraph:2100] Graph verify failed

we have our postproc kernel in host and c66. The cmd_status is -7 which means no resource. However the grap only have two node, tidl and postproc,  tidl is set on dsp1, postproc is set on dsp2.

thanks