Hi, TI team:
Due to customer requirements, we need to change the crystal oscillator of tad4 to 25MHz.
Please help guide how to modify it .
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI team:
Due to customer requirements, we need to change the crystal oscillator of tad4 to 25MHz.
Please help guide how to modify it .
Thanks
Hello Bangfei,
Please provide more information. What is the processor part number?
Regards,
~Leonard
Hello Bangfei,
I'm not finding any reference to PROC112A1 as a TI processor . Are you referring to the TDA4VM?
Regards,
~Leonard
The boot frequency cannot be changed. The device supports several different boot frequencies including 25Mhz, but the board design pin settings only supports 19.2MHz. There is a 2nd crystal input available and currently not populated. You can rework the board to add a 25MHz crystal (example part number is ABM10W-25.0000MHZ-8-J1Z-T3 or other device with same device footprint). This would allow a 2nd reference frequency into the processor. However the boot frequency will still be 19.2Mhz.
The board is populated with 19.2MHz, so the MCU_BOOTMODE[2:0] pins are set to '000' for 19.2MHz. If you change the WKUP_OSC crystal from 19.2MHz to 25MHz, yes the MCU_BOOTMODE[2:0] pin setting would need to change to '011' for 25MHz.
Thanks for your reply.
Now we want to change the crystal oscillator. Besides the modification of the MCU_BOOTMODE[2:0] pin on the hardware, do we need any modification on the software?
Thanks
We now change the crystal oscillator to 25MHz, and the MCU_BOOTMODE[2:0] pin is changed to 011.
Then use DFU to update the bin file, but he DFU device is not recognized.
Hi bangfei
Sorry for the long delay ,Does this issue still exists ?
Regards
Diwakar