Other Parts Discussed in Thread: OMAPL138, OMAP-L138, DA8XX, PMP
I am trying to get audio to play on my omapl138/DSP eval board using aplay built from dvsdk_omapl138-evm_4_02_00_06_setuplinux. It just hangs. Any ideas? Here is what I get:
root@arago:/# aplay -V stereo -v /var/audio/Blue.wav
Playing WAVE '/var/audio/Blue.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo
Plug PCM: Hardware PCM card 0 'DA850/OMAP-L138 EVM' device 0 subdevice 0
Its setup is:
stream : PLAYBACK
access : RW_INTERLEAVED
format : S16_LE
subformat : STD
channels : 2
rate : 44100
exact rate : 44100 (44100/1)
msbits : 16
buffer_size : 32768
period_size : 2048
period_time : 46439
tstamp_mode : NONE
period_step : 1
avail_min : 2048
period_event : 0
start_threshold : 32768
stop_threshold : 32768
silence_threshold: 0
silence_size : 0
boundary : 1073741824
appl_ptr : 0
hw_ptr : 0
+00%|00%+
Aborted by signal Interrupt...
This is where I press control-c