This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64GPEVM: Broken Synchronous Buck Controller U30

Part Number: TMDS64GPEVM

Dear Sir or Madam, 

we got three TMDS64GPEVM. 

With one of them I started to work and followed the Quick Start Guide. 

I was able to implement Linux on the AM64 and the board booted well. Then suddenly after 2 hours the board shut off and I could't power up on anymore. 

When the Board is supplied with 12V, LD6 and LD 12 are illuminated but if I switch SW1 to on, nothing happen anymore. 

I measured the EN2 Signal of U30. It's working well, when the switch is moved but the IC doesn't respond. 

What can I do? 

Best regards

Sebastian