Other Parts Discussed in Thread: ADS8556
Hi,
I am using a TI DSP C6713.
In the design, the McASP1 is connected to the control interface of ADC ADS8556
as well as the serial data interface.
I am trying to program the ADC ADS8556 using McASP and have a couple of questions.
1) Can we program the ADS8556 (precision A to D Converter) using McASP?
2) After initialization of McASP, I can see clock and framesync (probed on the respective pins
of ADS8556), but cannot see the data coming from the McASP Xmt pin of the DSP.
3) I think the reason could be that the McASP cannot function in clock-stop mode and so
it generates an error since the framesync and clock are continuous and since there is only one
control register in ADS8556, I transmit only one word on the McASP data lines.
Is this reasoning correct?
4) What is a possible way to program an ADC using McASP pins of C6713?
If possible can you guys give me some source code for McASP initialization for this case.
Thanks,
Aditi.